Other Parts Discussed in Thread: AM3359
CCSv6 TI PRU Cape for Beaglebone Black demo: compilation fails describes a problem where a example program for an AM3359 fails to compile from source. This example has:
- PRU programs compiled by the TI PRU compiler.
- The PRU programs are converted by the hexpru utility into an ARM "host image" ELF format file.
- The ARM "host image" ELF format files generated by the hexpru utility are referenced by the linker command file used by the TI ARM linker.
The problem is that the ARM "host image" ELF format files generated by the hexpru utility are rejected by the TI ARM linker with errors of the following form:
Running armofd on the ARM "host image" ELF format files generated by hexpru doesn't show a ".ARM.attributes" section. Is it the lack of a ".ARM.attributes" section which causes the ARM linker to assume the file is in TIABI_v0 format and therefore incompatible with the --abi=eabi ARM executable which is being generated?Building target: PRU_Demo.out
Invoking: ARM Linker
"/opt/ti/ti_ccs6_0/ccsv6/tools/compiler/arm_5.1.8/bin/armcl" -mv7A8 --code_state=32 --abi=eabi -me -O2 --define=am3359 --display_error_number --diag_warning=225 --diag_wrap=off -z -m"PRU_Demo.map" --heap_size=0x800 --stack_size=0x800 -i"/opt/ti/ti_ccs6_0/ccsv6/tools/compiler/arm_5.1.8/lib" -i"/opt/ti/ti_ccs6_0/ccsv6/tools/compiler/arm_5.1.8/include" -i"/opt/ti/AM335X_StarterWare_02_00_01_01/binary/armv7a/cgt_ccs/am335x/drivers/Release/" -i"/opt/ti/AM335X_StarterWare_02_00_01_01/binary/armv7a/cgt_ccs/utils/Release/" -i"/opt/ti/AM335X_StarterWare_02_00_01_01/binary/armv7a/cgt_ccs/am335x/beaglebone/platform/Release/" -i"/opt/ti/AM335X_StarterWare_02_00_01_01/binary/armv7a/cgt_ccs/am335x/system_config/Release/" --reread_libs --define=A8_CORE=1 --warn_sections --display_error_number --diag_wrap=off --xml_link_info="PRU_Demo_linkInfo.xml" --rom_model -o "PRU_Demo.out" "/home/Mr_Halfword/pru-software-support-package-pru-software-support-package/pru_cape/pru_fw/PRU_Audio/Debug/PRU_Audio_image.obj" "/home/Mr_Halfword/pru-software-support-package-pru-software-support-package/pru_cape/pru_fw/PRU_HDQ_TempSensor0/Debug/PRU_HDQ_TempSensor0_image.obj" "/home/Mr_Halfword/pru-software-support-package-pru-software-support-package/pru_cape/pru_fw/PRU_HDQ_TempSensor1/Debug/PRU_HDQ_TempSensor1_image.obj" "/home/Mr_Halfword/pru-software-support-package-pru-software-support-package/pru_cape/pru_fw/PRU_Hardware_UART/Debug/PRU_Hardware_UART_image.obj" "/home/Mr_Halfword/pru-software-support-package-pru-software-support-package/pru_cape/pru_fw/PRU_LED0/Debug/PRU_LED0_image.obj" "/home/Mr_Halfword/pru-software-support-package-pru-software-support-package/pru_cape/pru_fw/PRU_LED1/Debug/PRU_LED1_image.obj" "/home/Mr_Halfword/pru-software-support-package-pru-software-support-package/pru_cape/pru_fw/PRU_Switch/Debug/PRU_Switch_image.obj" "./pru.obj" "./pru_cape_demo.obj" "../pru_cape_demo.cmd" -l"rtsv7A8_A_le_eabi.lib" -l"drivers.lib" -l"utils.lib" -l"system.lib" -l"platform.lib"
<Linking>
fatal error #10183: --abi=eabi is incompatible with file "/home/Mr_Halfword/pru-software-support-package-pru-software-support-package/pru_cape/pru_fw/PRU_Audio/Debug/PRU_Audio_image.obj" (TIABI v0)
gmake: *** [PRU_Demo.out] Error 1