Other Parts Discussed in Thread: MSP430F5438A
Hello,
I am trying to get a printf(); statement to send a group of chars to the console. I used #include <stdio.h> and still no output. I cannot figure out how to change the heap or stack as some views suggested. there does not seem to be an option. Here is my code:
#include <msp430.h>
#include <stdio.h>
int main(void) {
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
P1DIR |= 0x01; // Set P1.0 to output direction
for(;;) {
volatile unsigned int i; // volatile to prevent optimization
P1OUT ^= 0x01; // Toggle P1.0 using exclusive-OR
printf("Hello world\n");
i = 10000; // SW Delay
do i--;
while(i != 0);
}
return 0;
}
The Target is the MSP430F5438A Experimenters board. It is hooked up with a FET430UIF debugger and a usb cable to the PC. I have tried sprintf() as well but nothing works. Thank