This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSV6.0 - Will it work with a TMS320VC5502?

Other Parts Discussed in Thread: TMS320VC5502

I have code for a TMS320VC5502 which complies using CCS v4.2.4, which was included in the TMS320C5502 eZdsp development kit. I am having difficulty moving to CCS V6.0. When trying to build the project (created using CCSV4), I get the following message:

"This project was built using a version of compiler that is not currently installed: 4.3.8 (C5500). Please go to CCS Application Center to install the compiler of this version, or migrate the project to one of the available compiler versions by adjusting project properties"

Furthermore, when I attempt to either "adjust project properties" or create a new project, the "Compiler Version" dialog box has no contents.

Suggestions?