This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Generating Sine Wave of 50Hz

Hello,

This is Sivakumar,

Im using a LM4F120 Stellaris Development Board to control the speed of the induction motor.

i need to generate a reference sinewave of  50Hz. How to do that?

Reply ASAP....

Regards

S.Sivakumar, Electrical Engineer

  • Hi Sivakumar,

    There is PWM Programming Example at the Tivaware Peripheral Driver Library Users Guide doc that you can learn from.

    There are also PWM example codes that you can learn from, which can be found at the Tivaware "\\examples\peripherals\pwm".

    - kel