Other Parts Discussed in Thread: HALCOGEN, TMS570LS3137
Hey,
I've got the following issue. I'm providing a custom bootloader, which loads an application through SCI. After building the application in CCS I'm creating an intel hex file with hex470. When the option "Enable PBIST Self Check" is disabled in HALCoGen the application is running well. I'm getting the following content in memory and hex file:
When PBIST Self Check is enabled, there are zeros at 0x0002A754 which do not appear in the generated hex file. See Screenshot:
Further Information:
HALCoGen version: 04.02.00
TMS470 HEX Converter: v4.9.9
Target: TMS570LS3137
How can I fix that?
Regards
Denis