Other Parts Discussed in Thread: CCSTUDIO
I a new user to CCStudio (v3.1) and recently added a header file to a project. The file is listed under the Include folder of the project, but when I double click on the file name or try to view properties CCStudio cannot find the file. The option to remove the file from the project is disabled, so I now cannot get rid of it from the Include folder list. Only after running into this problem did I consult the CCStudio IDE Help to learn that one should not attempt to manually add a header/include file. Unfortunately, it's too late. I've tried everything I can think of to resolve the issue without success. Does anybody have a suggestion for how I can delete this manually added include file from the project?
Thanks,
Bryan