Other Parts Discussed in Thread: MSP430F1611
Hello everyone.
Target Device:MSP430F1611.
Use Compiler : CCS v5
I have question
When I previously to compile the code that was used in CCS v4 in CCSv5 it is an error.
Partial an error has occurred is the part of Inline Assembler.
__asm("dtt_dcopy_loop:");
__asm(" swbp @R12");
__asm(" mov.w @R12+, 0(R13)");
__asm(" inc.w R13");
__asm(" inc.w R13");
__asm(" dec.w R14");
__asm(" jnz dtt_dcopy_loop");
These code was make error message.
I did not have any problem when you compile these codes in CCSv4.
These mnemonic uses what is described in the manual.
Error will occur when using the SWBP instruction.
When I use the SWBP instructions, error will also occur in the general assembler code.
I To use the Inline Assembler in CCSv5 is, do I need to set something to CSv5?
Error messages that occur are as follows.
"dtt.asm", ERROR! at line 1839: [E0002] Illegal mnemonic specified
swbp @R12
"dtt.asm", ERROR! at line 1861: [E0300] Symbol dtt_dcopy_loop has already been
defined
.dwpsn file "../dtt/dtt.c",line 1115,column 2,is_stmt
"dtt.asm", ERROR! at line 1862: [E0002] Illegal mnemonic specified
swbp @R12
"dtt.asm", ERROR! at line 1881: [E0300] Symbol dtt_dcopy_loop has already been
defined
.dwpsn file "../dtt/dtt.c",line 1115,column 2,is_stmt
"dtt.asm", ERROR! at line 1882: [E0002] Illegal mnemonic specified
swbp @R12
"dtt.asm", ERROR! at line 1913: [E0300] Symbol dtt_dcopy_loop has already been
defined
.dwpsn file "../dtt/dtt.c",line 1115,column 2,is_stmt
"dtt.asm", ERROR! at line 1914: [E0002] Illegal mnemonic specified
swbp @R12
"dtt.asm", ERROR! at line 1940: [E0300] Symbol dtt_dcopy_loop has already been
defined
.dwpsn file "../dtt/dtt.c",line 1115,column 2,is_stmt
"dtt.asm", ERROR! at line 1941: [E0002] Illegal mnemonic specified
swbp @R12
"dtt.asm", ERROR! at line 1961: [E0300] Symbol dtt_dcopy_loop has already been
defined
.dwpsn file "../dtt/dtt.c",line 1115,column 2,is_stmt
"dtt.asm", ERROR! at line 1962: [E0002] Illegal mnemonic specified
swbp @R12
best regards.