Hi All,
My platform is TM4C129
CCS version 5.5.0.00077
TivaWare-2.0.1.11577
I have included the graphic library
#include "grlib/grlib.h"
Then I add a function for test
But when the compiler in the linking stage,there are errors.
Description Resource Path Location Type
#10234-D unresolved symbols remain NNGT129 C/C++ Problem
#10010 errors encountered during linking; "NNGT129.out" not built NNGT129 C/C++ Problem
unresolved symbol GrContextInit, first referenced in ./MonitorCommand.obj NNGT129 C/C++ Problem
unresolved symbol GrContextFontSet, first referenced in ./MonitorCommand.obj NNGT129 C/C++ Problem
unresolved symbol GrCircleFill, first referenced in ./MonitorCommand.obj NNGT129 C/C++ Problem
unresolved symbol g_sFontCmss30b, first referenced in ./MonitorCommand.obj NNGT129 C/C++ Problem
unresolved symbol GrStringDraw, first referenced in ./MonitorCommand.obj NNGT129 C/C++ Problem
unresolved symbol GrRectFill, first referenced in ./MonitorCommand.obj NNGT129 C/C++ Problem
unresolved symbol GrRectDraw, first referenced in ./MonitorCommand.obj NNGT129 C/C++ Problem
I have no idea about this issue, if there are any advise, please let me know, thanks.