This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Using CCS 4 i don't see values of static and local variables even when debugging in same Module (C-File) or function.
With global Variables there is no problem. Also in CCS3 it did work fine. Is there any options to enable the acces to this symbols?
Michael
Version of CCS3: 4.1.1.00014
Target: TMS320F28035
Debugger: XDS510LC
Michael,
If the full symbolic debug is turned on and the optimizer is off, so the local variables are not stored in registers to increase efficiency, I don't see a reason why they are "disappearing". Are you sure you have these two options correctly configured?
Sometimes local variables can go away if they are never used in the routine, but I wonder if this is the case.
Hope this helps,
Rafael
Hi,
I have the same problem with ccs4 either
CCS Version: 4.1.1.00014
C2000 Compiler Settings:
Basic Options:
Debugging model: Full symbolic debug (--symdebug:dwarf, -g)
Optimization level: none
Device: TMS320F2809
Emulator: XDS510 USB
Code Example:
void do_test()
{
static BOOL_T is_error = MY_FALSE;
is_error = get_error_state();
if(is_error == MY_TRUE)
{
handle_error();
}
}
The static local var "is_error" to watch => identifier not found
Ed Rogalsky
Ki-Soo, could you elaborate a bit more, please? I am trying to debug a function which uses a variable named "threadbag" that's static to the module. I can find it in the "Modules" view, in the "Globals" section:
As you can see, there is no "$number" suffix. In fact, there are several "threadbag" variables because other modules have also a static variable with the same name, and there seems to be no means of telling to which module each variable belongs. I guess I could look at the memory address in the map file, but thst's quite a pain.
There are several symbols named "name$number" in the "Labels" section, but none of them have "threadbag" inside the name. Adding "threadbag" to the watch view brings the an "identifier not found: threadbag" error. Can you think of any practical workaround?
I am using CCS version 4.1.2.00027, the target is a C6455 and I'm debugging with the C6455 Device Cycle Accurate Simulator.
Thanks,
Pedro.
I am seeing the same problem (local and static variables not visible in debug) while using Code Composer 3.3.38
I too have Full Symbolic Debug enabled along with No optimization.
It is certainly frustrating. Is there a fix for this other than upgrading to a later version?
I am seeing the same problem in CCS 4; trying to debug a Stellaris application on LM3S8962 and several of my local variables do not appear in the debugger's "Local" view, and cannot be found using the "Watch" view.
Am using full symbolic debugging, with optimization set to 0. I don't see anywhere in the Modules view, however, that provides the $<number> mentioned in the post.
Has a resolution for this been determined?
Thanks,
David R.
I have the same problem like u either !
at last i found that if U do program like this .
you will not see values of static and local variables even when debugging in same Module!
Code Example:
void do_test()
{
{
static BOOL_T is_error = MY_FALSE;
.....//some other code
}
int a = 9;
}
The static local var "is_error" and 'a' to watch => identifier not found
U should try to code as below:
void do_test()
{
static BOOL_T is_error = MY_FALSE;
{
.....//some other code
}
int a = 9;
}
then u will see it!!!!!!
i suggest u check your code to make sure that there are not such cases in you program !
good luck!
Ki,
An update would indeed be great. I am using CCS 4.1.3.00038 and am having the same issue. Debugging is hard - if not impossible - as long as you have variables out there that you cannot inspect...
Best regards
Andreas
Changing the optimization level in Basic Options to "None" solved this issue for me. Earlier, the optimization level was set to "0", and I thought optimization is disabled. But from this thread (http://e2e.ti.com/support/development_tools/f/81/p/28346/100034.aspx) it seems to disable optimization you should choose "None" (or the blank option).
>>Yes I see this issue. You have to append a $<number> to the variable. You can find what that number from the Modules view (Window->Show View->Other->Debug->Modules). >>Looks like it means it's the second static variable.
How do we do this using CC 3.3?
I can confirm the same problem after so many years. What could I do to see the variables in the stack? I am using TI V6.4.4