This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cl6x stuck

Guru 10750 points

Hi All,

I'm trying to compile my project but it stuck in the linker stage with no warning or remarks,

[Linking...] "C:\Program Files\Texas Instruments\C6000 Code Generation Tools 6.1.9\bin\cl6x" -@"Debug.lkf"
<Linking>

The linker works only if I'm removing the below two pragma DATA_SECTION & DATA_ALIGN from the code, I tried to use only the DATA_SECTION but it doesn't help -

#pragma DATA_SECTION(GlobalBufferLoop, ".set_in_ddr2_global")
#pragma DATA_ALIGN(GlobalBufferLoop, 256)
short GlobalBufferLoop;

What could be the issue?

I'm using

CCS - Ver 3.3.82.10

CGT - v6.1.9

BIOS - 5.33.06

IDE - 5.98.0.393

Many Thanks,

HR