Hello...
I installed a fresh copy of CCS V6.0.1.00040 on WIN 7 and tried to created a new project. I selected the board ( eZDSP TMS320F28335) and selected the Spectrum Digital XDS510 USB emulator then I tried to verify the connection but I get the following:
Error parsing file:
Fatal Error at (0, 0): An exception occurred! Type:RuntimeException, Message:The primary document entity could not be opened. Id=C:\ti\ccsv6\eclipse///filer1.egr.msu.edu/cifs.homedir/dotwindows/workspace_v6_0/.tempFiles/testIdentify.ccxml
I know that the board and the JTAG are working because I checked them with another computer with the same operating system (WIN 7) and the same CCS version and the connection succeeded. I also checked the connection between PC and the JTAG via SdConfigEx v5 and the connection succeeded. I then uninstall CCS and installed it again but the same exact thing happened, I also updated but still no luck. How can I fix this problem?
Thanks!