This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flash programmer with CCS 3.1

Champs

 My customer is trying to install the flash programmer for CCS 3.1 and is getting the bleow error any help would be great.

 

I'm using the following  instructions to install the tool.

 

 http://c5000.spectrumdigital.com/evm5509a/docs/bsp/flashburn.html

FlashBurn is a utility included with Code Composer Studio that can be used to program code and data into the on-board Flash on the EVM5509A. One of the most common uses for FlashBurn is to take user code that has been debugged with Code Composer and program it into the Flash so that the board will boot it and run in standalone mode when it is powered up independently of the debug environment.

FlashBurn does not ship with standard configurations of Code Composer. However, it is available free of charge through Code Composers on-line Update Advisor. Use Update Advisor to download and install the FlashBurn install program.

This section describes how to burn a post into Flash using some pre-built example files, more detailed instructions on using FlashBurn can be found in the "FlashBurn Utility" section of the Code Composer Studio Online Help. The post and related files are in located in

c:\ti\boards\evm5509a\examples\post

The following sequence outlines programming the POST into Flash:

·         Create a bootloader image of the executable file in ASCII hex file format (post.hex).

·         Launch Code Composer Studio to allow access to the integrated tools.

·         Load the configuration document (post.cdd) that tells FlashBurn what to burn into Flash.

·         Erase the Flash with FlashBurn.

·         Program the Flash with FlashBurn.

Launching the update advisor , I get  the options below

Then I get the message below

 it is asking for a service code.

I am not sure what is the service code?

Thanks

Regards

Mohsen