This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Exporting projects to standard make file system



Hi Team,

In the manual of CCS V3.3, there is a section(Section 4.3.3) refers to export the project to standard make file format, which it can be build through GMAKE utility. It is also talks about DosRun.bat to set the environment.

Is there any availability of similar option in the new version?

I want to build the sample c project(with standard Makefile system) in DOS command prompt using c16x ti-compiler through command prompt. Please help me.Thanks in advance.

-Br,

Venki