Hello!
I'm a new CCS4 user. I've set up a target configuration for the XDS100 USB Emulator wtih the USB Stick 5505 device. I've saved the configuration and launched it. Under View->Debug, I see the following:
Texas Instruments XDS100 USB Emulator_0/C55xx [Non-Project Debug Session]
- Disconnected Device
-- Thread [main] (Disconnected(Unknown))
--- 0 <symbol is not available> 0x000000
Texas Instruments XDS100 USB Emulator_0/C55xx (9:16:03 AM)
Texas Instruments XDS100 USB Emulator_0/C55xx: CIO (9:16:03 AM)
Then I clicked on "Target->Connect Target". I get the following error:
C55xx: Error connecting to the target: Error 0x80000240/-604 Fatal Error during: Initialization, OCS,
I'm stuck at this point! Any ideas would be greatly appreciated!!
Thank you,
Robert