I have three redundant folders from project explorer, such as <5_SPI, 5_UARTA, 5_UARTB>, that is viewed I select the folder and right click and delete
CCV6 reported warning message on "problem view"
--------------------------
Description Resource Path Location Type
Invalid project path: Include path not found (H:\009-ADT-MyGIT\020-TI-F28335\SHRX_DMAF28335_1A\5_SPI). SHRX_DMAF28335_1A pathentry Path Entry Problem
------------------------- also apply to other folder.
I checked the Path and Symbol in project properties, there is no 5_SPI listed (because I previously remove it before), I checked other properties in advanced mode, but no sign of 5_SPI , 5_UARTA, 5_UARTB being listed or included.
How to fix this warning message?
Thanks.