This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debugger Errror

I am running Windows 8.1 x64 and I am using Stellaris LM4F120 Launchpad

I installed ccs v5.2 and I create the project as shown in the StellarisLaunchPadWorkbook. When I try to run the debugger I get the following error message:

Error initializing emulator: Error loading FTCJTAG.dll. Please make sure that the file exists (C:\ti\ccsv5\ccs_base\DebugServer\drivers\FTCJTAG.dll)

I checked for this file and it is there.