Hi,
I am using a Blackhawk USB560 JTAG emulator to connect to a EVMC6727 board (from DSP-Weuffen). I have upgraded to CCS4 and don't see a Board component for this device when configuring a Target. If it does not exist already, I would like to add the EVMC6727. I don't see an option for adding a new Board anywhere in the CCS4 GUI, so I am guessing I need to hand-craft an XML file. Is this the correct method of adding a new Board?
Thanks!