This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

unable to build any project in CCS after installation.

**** Build of configuration Debug for project fgfdg ****

"c:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../main.c'
'Invoking: C2000 Compiler'
"c:/ti/ccsv6/tools/compiler/c2000_6.2.7/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --include_path="c:/ti/ccsv6/tools/compiler/c2000_6.2.7/include" -g --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="main.pp"  "../main.c"
Command-line error: cannot open command file '\\0301616': No such file or directory
1 catastrophic error detected in this compilation.
Compilation terminated.

>> Compilation failure
gmake: *** [main.obj] Error 1
gmake: Target `all' not remade because of errors.

**** Build Finished ****

This is errors showing once i build the project. i have tried reinstalling the software too. Please tell me what to do next.

Regards

SURYA