This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

atan & atan2 function usage in TMS320f28377D



Hi,

In one of my application i am required to measure phase difference with an accuracy of 0.01degrees.I was using

this chip,& with the help of the atan function available in math.h, i am able to calculate the phase by giving phase(radians)=atan(y/x).

With this the phase value has a range from 0 to 89 & then -89 to 0, but i was having a requirement to get the phase in the range -180 to 180.

So i used atan2 function,when i used it the phase value does change in the range of -180 to 180,but the accuracy level seems to have dropped on comparing with atan with same values y & x as input & since in my requirement the accuracy is an important factor i was looking for a solution to this.

In CCS when i kept the floating point mode as strict,the accuracy increased a little but is not sufficient.

I am currently using compiler version V6.2.11.With v6.2.5 the output value of atan doesn't go beyond 45deg,with V6.2.9 & higher it gives -90 to 90 output with the same y,x values as input. 

would like to have some suggestions..