This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CG Tools C2000 6.4.2 Segfault on Compilation



The following Code crashes the compiler (for full code see attached files):

A get_a( uint16_t num ) {  return A(num); }

But it works written in two lines:

A a_from_b = b.get_a(3);
A* a = new A( a_from_b );

Compiler Arguments:

/ti-tools/ccsv6/tools/compiler/ti-cgt-c2000_6.4.2/bin/cl2000 -v28 -ml -mt --include_path="/ti-tools/ccsv6/tools/compiler/ti-cgt-c2000_6.4.2/include"  --preproc_with_compile  main.cpp

Error Message:

INTERNAL ERROR: /home/dirk/light/ti-tools/ccsv6/tools/compiler/ti-cgt-c2000_6.4.2/bin/ac2000 experienced a segmentation fault
while processing function main file main.cpp line 38

This is caused by a defect in the compiler itself. TI Customer
Support may be able to suggest a workaround to avoid this.

Upgrading to the newest version of the compiler may fix this problem.

Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler". See the link titled
"Submitting an issue". Include this ENTIRE error message and a
copy of the .pp file created when option --preproc_with_comment
(-ppc) is used.

main.cxx