This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Devices and features supported in CCSv6 Node locked license

Hi,

I want to purchase Code Composer Studio v6 node locked license.

Before that I want to know that, if I buy node locked license, can I use it to develop applications on all the processors/microcontroller families like TMS320F28xx, TMS470, TMS570, DM816x etc.?

OR

I have to buy license for each family separately?

Does it support all the debuggers like Blakhawk XDS100v2, Spectrum digital USB510 etc.?

Does it support OS like Windows XP, Windows7/8 32-bit/64-bit?

regards

Lingaraju 

  • Hello

    Lingaraju CH said:
    Before that I want to know that, if I buy node locked license, can I use it to develop applications on all the processors/microcontroller families like TMS320F28xx, TMS470, TMS570, DM816x etc.?

    Yes. A single node-locked full license can be used with ALL devices supported by Code Composer Studio.

    Lingaraju CH said:
    Does it support all the debuggers like Blakhawk XDS100v2, Spectrum digital USB510 etc.?

    Yes. A single node-locked full license can be used with ALL debug connections supported by Code Composer Studio

    Lingaraju CH said:
    Does it support OS like Windows XP, Windows7/8 32-bit/64-bit?

    Yes. A single node-locked full license can be used with ALL Host OS supported by Code Composer Studio. So this includes CCS for Linux also.

    Thanks

    ki