With CCS 6.1.0.00104 running under CentOS 6.5 64-bit, was attempting to use a Segger J-Link with J-Link support v0.1.0.4 to debug a EK-TM4C1294XL.
However, CCS is repeatably crashing when attempt to start a debug session. From the progress indications prior to the crash the target is successfully programmed.
Attached is a CCS crash dump file and Debug Server log for a crash.
The Segger J-Link and EK-TM4C1294XL are OK, since can use with with CCS 6.0.1 under Windows 7 with the Windows J-Link support v0.1.0.5
[The latest version of J-Link support for Linux is v0.1.0.4 and for Windows is v0.1.0.5, which is the reason for the different versions used]