This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connection Problems with multiple USB devices - MSP430 & LM3S3748



All:

I use the 3748 as an oscilloscope. When I connect the MSP430 JTAG, I cannot communicate using CCS4.1, IF I also have the 3748 connected. The 3748 is NOT being connected to CCS 4.1, only to the Oscilloscope GUI.

However, I can connect IAR tools to the MSP430 JTAG and RUN the oscilloscope function of the 3748.

Is there a planned fix for this problem?

Regards,

Todd Anderson