Other Parts Discussed in Thread: MSP-FET, MSP430F5438A
Hi,
I 'm trying to use the msp-fet but with no success. I installed ccsv6 as preconize, but when i launch the debugger with the following target :
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="TI MSP430 USB1_0">
<instance XML_version="1.2" desc="TI MSP430 USB1_0" href="connections/TIMSP430-USB.xml" id="TI MSP430 USB1_0" xml="TIMSP430-USB.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="TI MSP430 USB1_0">
<instance XML_version="1.2" href="drivers/msp430_emu.xml" id="drivers" xml="msp430_emu.xml" xmlpath="drivers"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="MSP430F5438A_0" href="devices/MSP430F5438A.xml" id="MSP430F5438A_0" xml="MSP430F5438A.xml" xmlpath="devices"/>
</platform>
</connection>
</configuration>
</configurations>
I have the error : "Error initializing emulator: Interface Communication error"
Before that I work with MSP-FET430UIF and ccsv4 without problem...
regards,
Mathieu