Other Parts Discussed in Thread: CCSTUDIO
Hi,
I am trying to use the Tools/Graph feature for sanity-checking my data.
When i select Tools/Graph/Single time in the menu, I get a very brief (say 0.2s)
glimpse of the "pie" busy cursor before it reverts to the regular arrow and ccs freezes.
The same actions in ccsv5,5 brings up a dialog asking for format, address etc of data to
display and brings up a graph window.
I am currently using CCS 6.1.0.00104 on a fully updated Ubuntu 14.10 machine.
Target is an EVMK2H rev 3.0
I did note a line on the Linux console from which the ccstudio was started saying
"dvtLogOptions.xml DOES NOT exist".
Tried the same Tools/Graph thing with a colleague using a similar target (including FFTC) with same result.
Suggestions?
br
/Anders