This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to solve the Error connecting to the target: (Error -151 @ 0x0)



Hi, I am using the F28M35H52C1 with CCS 5.1.5, and when I try to connect Targe I get this issue:

Error connecting to the target:(Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif'folder to verify the emulator can be located.

I have also reinstalled CCS. Can anyone tell me why this is happening?

Thanks,

Mahesh