This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error generated by TI's USCIF driver or utilities '-183' (0xffffff49).

Hi,

I am not able to connect to DSP using emulator. I am getting following error. I have checked the connectivity  and power are proper.

[Start: Blackhawk USB560-M Emulator_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\kruthika\AppData\Local\Texas Instruments\
CCS\ti\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560usbm.out'.
The library build date was 'Mar 9 2014'.
The library build time was '22:35:20'.
The library package version is '5.1.450.0'.
The library component version is '35.34.40.0'.
The controller does use a programmable FPGA.
The old VHDL code has a version number of '0' (0x00000000).
The new VHDL code has a version number of '386336272' (0x17070610).

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-183' (0xffffff49).
The title is 'SC_ERR_CTL_CBL_BREAK_FAR'.

The explanation is:
The controller has detected a cable break far-from itself.
The user must connect the cable/pod to the target.

[End: Blackhawk USB560-M Emulator_0]