This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv4 cannot go between real-time and regular mode dynamically



CCSv4's real-time mode options are provided in such a place that it is no longer possible to toggle between real-time mode and regular (non real-time) mode when target is already launched. It requires relaunching the target. CCS 3.3 used to allow dynamic switching which is quite convenient and useful during system software debugging. So CCSv4 should retain this capability. Please file this as an enhancement request although it can be looked as a bug when seen relative to 3.3 (and this I believe has nothing to do with eclipse standard compliance). An appropriate place to add this feature seems to be in the Target menu, where things like single step etc are there.