Other Parts Discussed in Thread: CCSTUDIO
Hey forum,
I'm using CCS3.3 along with a TMS320C6713 DSK to program a graphic equalizer for a project. I wish to be able to include cut/boost in the equalizer so I need fractional increments for gain in my slider gels (0.1 gain=-10dB attentuation). However, everytime I try to use a non integer I get an error when loading the GEL stating:
GEL: Error loading file 'C:\CCStudio_v3.3\MyProjects\sine8_LED\gain.gel': line 6: expecting IntegerConstant, found '0.1'
I've tried redifining the gain variable associated with the slider in the C code to a float or decimal but I've had no luck. I am assuming the integer constant association involves the code for the slider gel commands themselves. All I could find is a .dll file associated with the slidergel usage but have no way of editing it. Is there any way I can use a fraction for the increment values with slider gels? A work around could be just multiplying my gain factor in the C code by 0.1 but I'd rather avoid this route