This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help for some compilers is not displayed by CCS 6.1, even though installed

On CCS 6.1.0.00104 installations on both Windows and Linux, I have noticed that the help for some compilers is not displayed even though the compiler help is reported as installed.

E.g. the following from the Code Composer Studio Installation Details reports that help for all compilers is installed:

Yet the CCS help doesn't show the ARM or C2000 compiler help:

In the CCS Eclipse log I noticed the following messages for the ARM and C2000 compiler help which is not being displayed:

!ENTRY org.eclipse.equinox.p2.publisher.eclipse 4 0 2015-03-15 10:56:18.143
!MESSAGE Unable to acquire PluginConverter service during generation for: /opt/ti/ti_ccs6_1/ccsv6/eclipse/plugins/com.ti.cgt.c2000.6.4.help_6.4.0.

!ENTRY org.eclipse.equinox.p2.publisher.eclipse 4 0 2015-03-15 10:56:19.637
!MESSAGE Unable to acquire PluginConverter service during generation for: /opt/ti/ti_ccs6_1/ccsv6/eclipse/plugins/com.ti.cgt.arm.5.2.help_5.2.0.

!ENTRY org.eclipse.equinox.p2.publisher.eclipse 4 0 2015-03-15 10:56:31.696
!MESSAGE Unable to acquire PluginConverter service during generation for: /opt/ti/ti_ccs6_1/ccsv6/eclipse/plugins/com.ti.cgt.c2000.6.4.help_6.4.0.

!ENTRY org.eclipse.equinox.p2.publisher.eclipse 4 0 2015-03-15 10:56:32.458
!MESSAGE Unable to acquire PluginConverter service during generation for: /opt/ti/ti_ccs6_1/ccsv6/eclipse/plugins/com.ti.cgt.arm.5.2.help_5.2.0.


This is only an annoyance, as the TI Compiler documentation is available as separate PDF files, but am reporting it in case it is a sign of some Eclipse PlugInConverter issue which could affect other CCS Eclipse plug-ins.