I just installed CCS and had the wizard create a New Project for a CC2650. I selected the 'Empty Project (with main.c)' which says it will create a project fully initialised for the selected device.
However the generated project fails to link because ResetISR isn't defined. I can see what's wrong here, there's no startup file with the routine in it . All that appears to be in the CC26xxWARE pack. Was there another component I was supposed to add to CCS to get the wizard to generate a really complete example project, or do you need to put all the pieces together by hand, add CC26xxWARE to the include path, import the starter file, fix up the linker maps etc?
Also, is there a package of examples for the CC2650 devkit which I've not found yet? Expected there to be a blinky sample, some peripherals examples etc, all simple snippets with a CCS project to build them, just to get started. But I've found nothing yet, I must surely have been looking in the wrong place, a package of getting started examples is pretty common .. no?