I recently uninstalled Code Composer version 5.4 and tried to install version 5.5 instead. I had issues with the uninstaller where it would say something about the "--mode" parameter being incorrect. I ended up renaming the folder containing that installation to TI_old, and installed Code Composer version 5.5 in a new TI folder. I installed TivaWare_C_Series-2.1.0.12573 in the same directory and attempted to create a new Code Composer project to work with the TM4C1294XL board. However as I was working on this project I had issues with the trackpad on my laptop that I don't believe were related to Code Composer. I saved my work and restarted my computer. Now the issue with the trackpad has been resolved but when I launch Code Composer a message notifies me that an error has occurred and that I should check the log file at: workspace\.metadata\.log. I have looked at the log but I am unsure what to make of it, I was wondering if anyone could help me figure out what is going on. I have posted the error report here:
. Thanks in advance.