This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS Compilation error 'UNC Path not found'

Hi,

I am using windows 7 64-bit and installed CCSv5.5.

I got the copy of C project from the server and run it on my computer without any issue. After making a change in the code, when I try to build it; it shows following error:

{ "C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all

'\\tuls00810\Users\sl101934\Documents\C Code\QuartzFSK-rev1.00\Debug'

CMD.EXE was started with the above path as the current directory.

UNC paths are not supported. Defaulting to Windows directory.

'Building file: ../main.c'

Fatal error #1965: cannot open source file "../main.c" }

Can you please help resolving this issue.

Regards,

Sukirti.