This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

blackhawk usb560v2 failed to connect LCDKC6748

Hi there,

I added a new configuration file to my project to use BH560V2 emulator but failed in connection (The project was running well using XDS200). I'm using CCS 6.0.1.00040.

Here is the error report:

************************************************************************************************************************************************

[Start: Texas Instruments XDS560 Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\rebeccaz\AppData\Local\TEXASI~1\
CCS\ti\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'xds560.out'.
Failed to open i/o connection (\\.\xds5600)

An error occurred while soft opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.

The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.

[End: Texas Instruments XDS560 Debug Probe_0]

**********************************************************************************************************************************************

No such error code '-250' found in blackhawk datasheet. 

Can any one tell me what is this error and how to fix it?

Thanks!

Rebecca