Hallo,
I try to use the On-Chip Flash Programmer which is available in CCS v3.3 to debug the Flash version of my Application firmware.
I use the FlashAPIInterface28335V2.10 with the file FlashAPIInterface28335V2_10.out.
I get alway error messages (attached pdf), but at least the delete Flash function does the job, the flash is empty.
The same error messages I get while programming my Application, but it will not work.
With the Flash Tool from Blackhawk FlashBurn v3.1 all is working fine, this tool uses also the API 2.10.
What could cause this errors?
Is there another possibility to debug my Flash Application?
Ralf
see attached fileCCSv3.3 FlashProgramingTool F28335.pdf