Hi,
I'm having an issue where it seems that the text inside of the text editor gets out of sync with the IDE or screen.
As a result I have issues where it's giving me errors about my syntax, but the text editor doesn't display my information correctly so I can't fix it.
Below is a picture where line 18 has a syntax error, but is not being display properly:
This picture was taken after I performed the following:
1. Closed Code Composer Studio
2. Reopened Code Composer Studio
3. Performed a clean of the project
4. Compiled the project
The only way I have found to fix the issue is to totally restart my computer.
I am running Code Composer Studio Version: 6.1.0.00104.
The OS is Windows 7 64-bit, Service Pack 1.
Any hints on what could be causing the issue, or how to solve it other than a complete restart?
Thanks,
Ben