Other Parts Discussed in Thread: ENERGIA, TM4C123GH6PM
Hello everyone,
So yesterday I had some peps using CCS for the first time. But some of them encountered problems that I could not solve at the time and could not reproduce in my computer later.
This was using CCS V6.1.0 and importing Energia sketchs from v15.
1 problem was:
- 1 computer could build fine but when tried to debug it gave the error, now bare with me that I can't check so I have to say on the top of my head, "could not find symbol "setup" ".
- Then 2 computers had the problem that they couldn't control the program flow on the board. It connected to the board but simply the play, pause, step over, etc were all grayed out.
I checked on all computers and the drivers seemed fine.
Also 1 problem I have in CCS on linux:
Every time I use simple perspective the IDE ends up crashing. Not only that while working the drop down windows show 1 or no options to select (like "projec" does not show anything to select", nor "file")
I can try to ask for more info on the OS and such. Is there any solution to these problems or some are known bugs?
Sorry if I couldn't give out more information right of the bat