Hi all,
I'm using GNU v4.9.1 compiler, and I'm just trying to work with WDT timer:
void __attribute__((interrupt(WDT_VECTOR))) WDT_ISR(void)
{
P2OUT ^= BIT1;
}
When trying to build it, I keep gettign these errors:
section `__interrupt_vector_11' will not fit in region `VECT11'
region `VECT11' overflowed by 2 bytes
Do you have any idea, what could cause this?
Thanks.