I have an issue updating the compiler for the MSP430 in CCS 5.5. We have several MSP430 projects and several developers. We need each developers PC to build each project using the compiler that is configured in the project properties. If we change compilers, we need to perform complete regression testing. We have been bitten by that in the past.
So, for example, one of our developers has CCS with compiler version 4.2.1 installed. The project is in revision control and was built with compiler v4.2.2.
When I check Help->Check For Updates or Help->Add New Software, I am only offered compiler version 4.2.7 for the MSP430.
I NEED compiler version 4.2.2..
How do I get CCS 5.5 to offer the intermediate updates, NOT just the latest?
See attached screen shots.
Jim