This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

hyperlink



Can I insert a hyperlink to a local file in the standard CCS6.1 C/C++ editor? Specificaly I would like to insert a link to an Excel file or a Visio file.

  • Richard Conti said:
    Can I insert a hyperlink to a local file in the standard CCS6.1 C/C++ editor?

    I haven't found a way to insert hyperlinks using the built-in editor, but you could create the file using another editor that supports hyperlinks and add the file to a CCS project. For instance, if I have a Word doc that is part of a CCS project I can double-click on it in the Project Explorer view to open it in CCS and click on the hyperlinks.