This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't connect to F28075 ControlCard

Hi there, 

For a project, we bought two F28075 ControlCard Kits. We started developing on one, while having the other in back-up. We wanted to do some testing on the other kit aswell, but we're having trouble to connect to it and receive the following error:

"Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 5.1.641.0)"

We're having no problem running the code on the first device, but when we try and connect to the other board (not two boards at once), it gives the error.

The setup is identically the same: same usb-cables, same switches set on the ControlCard (for reference: A:SW1 pos 1 is set to ON, A:SW1 pos 3 is OFF, SW1 pos 1 is OFF, SW1 pos 2 is ON).

Maybe I'm missing some step, that I didn't realise I did, when I set up the first one?

I hope you can help :)

Kind regards,

Carl