Other Parts Discussed in Thread: MSP430F5437
Hello,
I'm trying to port Contiki (http://www.sics.se/contiki/) for my own board which contains a MSP430f5437.
As I have a MSP430 USB-Debug-Interface (MSP-FETU430IF) which works well with CCS4 (4.1.1.00014), I'm editing the code on CCS4.
As Contiki has its makefiles, I created a "Standard Make Project". The compiler is mspgcc4 (http://mspgcc4.sourceforge.net/).
I can compile the code using mspgcc4, but when I try to make a debug session CCS4 fails to recognise the binary file that I give to it (Debug Window > Main > C/C++ Application). The error message is "Program is not a recognized executable."
Using Cygwin, I checked the file format of the binary file which gives :
-------------
$ file contiki/examples/hello-world/hello-world.wlsn4u
contiki/examples/hello-world/hello-world.wlsn4u: ELF 32-bit LSB executable, version 1, statically linked, not stripped
-------------
but when I check the file format of the binary file generated by a "regular" project with CCS4 (File > New > CCS Project), I get :
-------------
$ file hello/Debug/hello.out
hello/Debug/hello.out: data
-------------
So as I don't have the same binary format, it's normal that CCS4 doesn't recognise my binary file. But how can I have it recognised ?
Do you know if there is an option somewhere in mspgcc4 or in CCS4 that I can use for that ?
Or simply, it is possible to use mspgcc4 to compile code that CCS4 will use for loading the processor and debugging it ? If not, is there a way to use the USB-Debug-Interface with another tool ?
Thanks.
Best,
Yorick