Other Parts Discussed in Thread: CC430F5137
Hi
I am using ubuntu 14.04 64 bit on virtualbox on Windows 8.1 64 bit host.
I have to build some project and the project uses cmake system. I need to cross compile my project for cc430f5137 and for this i require msp430 gcc.
I downloaded the msp430-gcc-full-linux-installer-3.2.3.0.run file as mentioned here .
when i downloaded then I did
sudo chmod +x msp430-gcc-full-linux-installer-3.2.3.0.run
then when I type
./msp430-gcc-full-linux-installer-3.2.3.0.run
nothing happens and I get a new line on terminal.
if I type
sh ./msp430-gcc-full-linux-installer-3.2.3.0.run
then I get the following error
./msp430-gcc-full-linux-installer-3.2.3.0.run: 1: ./msp430-gcc-full-linux-installer-3.2.3.0.run: Syntax error: "(" Unexpected
Even if I double click the.run file from the files directory, nothing happens
i am new to linux and I am doing this for the first time. I have searched the internet but I havent found anything useful.
Please help me in setting up the msp430 gcc tool chain
Thanks