We purchased code composer studio 6 IDE, Floating 1 User Pack about 6 months ago.
On Thursday May 6, I opened the shrink wrap, used the CD to install, and performed the activation procedure using the TI Activation ID inside the shrink wrap and the MAC address of my computer. I received the license file by email, installed it, and the license displayed changed from Free License to show that it was now fully licensed, and it allowed use of my USB510 emulator. (In retrospect, this is perhaps surprising, since I did not try to install it on a license server.)
During the weekend, there was a power outage and my computer performed a reboot. When I tried to enter code composer 6, it asked my to do an installation. I reinstalled from the CD (uninstall did not work by the way). This went OK, and the free version worked OK. But when I entered the license file, it politely ignored this and continued to operate from the free license only.
I have tried getting a new license file, rehosting (with the same MAC address), but nothing works. I have also tried the free 90 day evaluation, but this also does not work...says that it has already been used, which I do not think is true, since I have always used only version 3.3 of code composer until now.
In short, we purchased this product for $750, and after about 10 hours of tinkering, I have nothing that works. Sort of disappointing after so many years of good experience with Code Composer 2 and 3.
What can I do to get Code Composer 6 running as quickly as possible?
Thanks