Hi,
I have a project using CCS6.1that has been building fine with no errors. However, today three errors are generated, but it creates the output file successfully. The errors are for assigning a variable to itself (x = x;) and the error icon is not the usual icon, it is what appears to be a red bug (see image below).
I checked the MISRA options, but none are enabled...is there another place where additional error conditions can be enabled? I'm wondering if someone in my group inadvertently turned some on.
Thanks,
David