This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Blackhawk USB100v2 connection problem

I'm trying to programming TMS570 with blackhawk USB100v2 . I'm using the Ti 14 pin connection and I'm connecting pin to pin as follows.

Whenever I launch the debugging session on code composer studio I get the following error:

When testing the connection I get the following log:

[Start: Texas Instruments XDS100v2 USB Emulator_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\GOG\AppData\Local\TEXASI~1\CCS\
ti\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'May 21 2014'.
The library build time was '17:19:59'.
The library package version is '5.1.507.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-183' (0xffffff49).
The title is 'SC_ERR_CTL_CBL_BREAK_FAR'.

The explanation is:
The controller has detected a cable break far-from itself.
The user must connect the cable/pod to the target.

[End: Texas Instruments XDS100v2 USB Emulator_0]

What should I look for when making the connection. Am I doing the right connections?

I would appreciate if you can help.