Other Parts Discussed in Thread: CCSTUDIO
I am trying to run a MATLAB built C code in CCs V3.3 there is an error as:
error: symbol referencing errors - './Debug/right.out' not built
Warning: The project has no cmd file while the Text Linker is selected
[Linking...] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -@"Debug.lkf"
I would like to know the procedure and solution for running the file.
There is no compilation error shown and the above displayed error is during the project build process, to create (executable) .out file