This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, I have been having problems with CCS getting stuck on a gmake: access is denied. error for several days now. I have read several other forums on this issue but the answers are not really conclusive. I disabled Kaspersky and that worked for a while. Today I was having the same error with Kaspersky disabled but I was able to get it running by restarting CCS. However, I now need to build two projects one for each CPU. I was able to build the first project but when I try to build the second project it is stuck on gmake: *** waiting for unfinished jobs. I cannot restart CCS because I will lose my cpu1 build. Can someone look into how to fix this?
Adam,
Are you still hitting this issue? In the past when others have hit this type of issue, disabling the anti-virus was sufficient to resolve the problem. I'm not really sure what else it could be if you have already disabled the anti-virus.
I think the issue still exists. At some point I was able to get the program to build without making any additional changes. The problem is intermittent. I have not run any programs for a few days but I expect to see this problem in the future because I have not changed anything in the system.
I had this issue as well. Disabling the antivirus didn't work for me. Instead, the problem was windows firewall. To solve it, i went to "Start" and typed "Firewall". After that, clicked "Allow a program through Windows Firewall" and clicked on "ccstudio" on the new window.
Hope it helps.
Regards.