This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code composer - Windows update problem

We are running Code Composer v 3.3.82 on several PCs.

Operating system is Windows XP SP3.

After running Windows Update on 2 of these PCs, Code Composer refuses to take contackt with emulator, reporting "target power error".

The Udpdate was cumulated from the past two weeks, until today, April 21th 2010.

 

  • Hi,

    Can you post the complete error or screenshot of the same?

    Problem could be anything from CCS corruption to emulator drivers corruption thus requiring fresh installation after registry cleanup possibly.

    A detailed error log or screenshot could help.

    Regards,

    Sid

     

  • False alarm. Two of our DSP cards and one of our emulators were destoyed at the same time. Unbelievable unluck. ( Because of static discharge? )

    The error had nothing to with windows update.