Other Parts Discussed in Thread: TM4C1294NCPDT, ENERGIA, EK-TM4C1294XL, LMFLASHPROGRAMMER, UNIFLASH
Code Composer Studio Version: 6.1.0.00104
OS: Linux Mint 17.1 Cinnamon 64-bit Version 2.4.8
Target board: Tiva TM4C1294NCPDT
In setting up my first project I attempted to "test" the connection on the "General Setup" tab and received the following in a pop window:
[Start: Texas Instruments XDS110 USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
/home/dbristow/.ti/ti/0/0/BrdDat/testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'libjioxds110.so'.
The library build date was 'Feb 19 2015'.
The library build time was '02:33:39'.
The library package version is '5.1.641.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.
The explanation is:
An attempt to connect to the XDS110 failed.
The cause may be one or more of: invalid firmware update, invalid
XDS110 serial number, or faulty USB connection. The firmware and
serial number may be updated using the xdsdfu utility found in
the .../ccs_base/common/uscif/xds110 directory of your
installation. View the ReadMe.txt file there for instructions.
[End: Texas Instruments XDS110 USB Debug Probe_0]
from a terminal I run lsusb
dbristow@stjean ~/myApps/ti/ccsv6/ccs_base/common/uscif/xds110 $ lsusb
Bus 002 Device 013: ID 1cbe:00ff Luminary Micro Inc. Stellaris ROM DFU Bootloader
Bus 002 Device 002: ID 8087:0024 Intel Corp. Integrated Rate Matching Hub
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 004: ID 04b3:3025 IBM Corp. NetVista Full Width Keyboard
Bus 001 Device 003: ID 046d:c52b Logitech, Inc. Unifying Receiver
Bus 001 Device 002: ID 8087:0024 Intel Corp. Integrated Rate Matching Hub
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
then xdsdfu
dbristow@stjean ~/myApps/ti/ccsv6/ccs_base/common/uscif/xds110 $ ./xdsdfu -e
USB Device Firmware Upgrade Utility
Copyright (c) 2008-2014 Texas Instruments Incorporated. All rights reserved.
Scanning USB buses for supported XDS110 devices...
<<<< Device 0 >>>>
VID: 0x1cbe PID: 0x00ff
Device Name: Device Firmware Upgrade
Manufacturer: Texas Instruments
Serial Num: 0.1
Mode: DFU
Found 1 device.
I've followed the instructions in the ReadMe.txt in the xds110 directory.. to no avail! oh except now I Energia can't find the port!
I've tried to find a solution in this forum and many response to USB issues I've looked at, I've uninstalled and reinstalled the drivers..